earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Device Administrator, AS-P
Functionalities: Basic Functionality
Product version: 3.2, 3.3, 2022
10/15/2020

Uninstalling Device Administrator

You uninstall Device Administrator to permanently remove the application from your computer.

Show More
action_close

To uninstall an EcoStruxure Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the EcoStruxure Building Operation product from the computer or server.

Notice

Loss of data

Return all activated network licenses to the License Activation Server before uninstalling the License Server and License Administrator. Licenses cannot be returned without a License Administrator. For more information, see Removing an EcoStruxure Building Operation Software Demo License .

Failure to follow these instructions can result in loss of data.

Notice

Loss of data

Back up the EcoStruxure BMS server before uninstalling the product. All​ user settings, database information, and system files related to this product are erased. Files and backups created by the user remain and are not erased. For more information, see Backing Up EcoStruxure BMS Servers Manually .

Failure to follow these instructions can result in loss of data.

Client tools and language packages are uninstalled together with the uninstallation of WorkStation.

To uninstall Device Administrator
  1. In Windows Control Panel, select Schneider Electric EcoStruxure Device Administrator Building Operation x.y and then click Uninstall .

  2. In the Device Administrator x.y Uninstall dialog box, click Uninstall .

  3. Click Close .

    Note:

    Click Show details to follow the progress of the installation.

  • Uninstallation
  • Products
  • Stopping the Enterprise Server Windows Service