earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Device Administrator, AS-P
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Uninstalling Device Administrator

You uninstall Device Administrator to permanently remove the application from your computer.

显示更多
action_close

To uninstall an EcoStruxure Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the EcoStruxure Building Operation product from the computer or server.

通知

数据丢失

Return all activated network licenses to the License Activation Server before uninstalling the License Server and License Administrator. Licenses cannot be returned without a License Administrator. 有关更多信息,请参阅 Removing a Local License or Returning a Network License .

不遵照这些说明可导致数据丢失。

通知

数据丢失

Back up the EcoStruxure BMS server before uninstalling the product. All​ user settings, database information, and system files related to this product are erased. Files and backups created by the user remain and are not erased. 有关更多信息,请参阅 Backing Up EcoStruxure BMS Servers Manually .

不遵照这些说明可导致数据丢失。

Client tools and language packages are uninstalled together with the uninstallation of WorkStation.

To uninstall Device Administrator
  1. In Windows Control Panel, select Schneider Electric EcoStruxure Device Administrator Building Operation x.y and then click Uninstall .

  2. In the Device Administrator x.y Uninstall dialog box, click Uninstall .

  3. Click Close .

    注释:

    Click Show details to follow the progress of the installation.

  • Uninstallation
  • Products
  • Stopping the Enterprise Server Windows Service