earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Ratgeber

Ratgeber


Produkte: License Administrator
Funktionen: Basisfunktionalität
Produktversion: 1.8, 1.9
20.05.2015

Uninstalling the License Administrator

You uninstall License Administrator to permanently remove the application from your computer.

Hinweis

Loss of data

Return all activated network licenses to the License Activation Server before uninstalling the License Server and License Administrator. Licenses cannot be returned without a License Administrator. Für weitere Informationen siehe Removing a Local License or Returning a Network License .

Failure to follow these instructions can result in loss of data.

Mehr zeigen
action_close

To uninstall a Building Operation product you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the Building Operation product from the computer or server.

Hinweis

Loss of data

Return all activated network licenses to the License Activation Server before uninstalling the License Server and License Administrator. Licenses cannot be returned without a License Administrator. Für weitere Informationen siehe Removing a Local License or Returning a Network License .

Failure to follow these instructions can result in loss of data.

Hinweis

Loss of data

Back up the Enterprise Server before uninstalling the product. All​ user settings, database information, and system files related to this product are erased. Files and backups created by the user remain and are not erased. Für weitere Informationen siehe Backing Up SmartStruxure Servers Manually .

Failure to follow these instructions can result in loss of data.

Client tools and language packages are uninstalled together with the uninstallation of WorkStation.

To uninstall the License Administrator
  1. On the Windows toolbar, select Start , and then click Control Panel .

  2. Click Uninstall a program .

     
    action_zoom_plus_stroke
  3. Select Schneider Electric StruxureWare Building Operation License Administrator and then click Uninstall .

     
    action_zoom_plus_stroke
  4. Click Uninstall .

     
    action_zoom_plus_stroke
  5. Click Close .

    Hinweis

    Click Show details to follow the progress of the installation.

     
    action_zoom_plus_stroke
  • Uninstallation
  • Products