earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Alarmes
Version produit : 2.0, 2.1, 3.0, 3.1
18/05/2018

Unit of Measure in Alarms

When creating an alarm, the alarm limit and deadband values inherit the unit of the monitored variable. You can change the unit of the alarm to any unit within the same unit category as the monitored variable.

Déclaration

You cannot define a unit to an alarm that monitors a unitless variable.

If the unit of a monitored variable is replaced by a unit within the same unit category as the unit of the alarm, the EcoStruxure Building Operation software automatically handles the conversion. If the unit of the monitored variable is replaced by a unit that belongs to another unit category, the alarm is disabled by the EcoStruxure Building Operation software. The EcoStruxure Building Operation software triggers a system alarm to notify that the alarm is disabled due to an impossible unit conversion.

  • Alarm Functions
  • Alarms Overview