earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/2

Unit of Measure in Alarms

When creating an alarm, the alarm limit and deadband values inherit the unit of the monitored variable. You can change the unit of the alarm to any unit within the same unit category as the monitored variable.

注释:

You cannot define a unit to an alarm that monitors a unitless variable.

If the unit of a monitored variable is replaced by a unit within the same unit category as the unit of the alarm, the EcoStruxure Building Operation software automatically handles the conversion. If the unit of the monitored variable is replaced by a unit that belongs to another unit category, the alarm is disabled by the EcoStruxure Building Operation software. The EcoStruxure Building Operation software triggers a system alarm to notify that the alarm is disabled due to an impossible unit conversion.

  • Alarm Functions
  • Alarms Overview