earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Localization
Product version: 2.0, 2.1, 3.0, 3.1
10/30/2018

Select Unit Dialog Box

Use the Select Unit dialog box to define the unit and metric prefix of a value.

 
action_zoom_plus_stroke Select Unit dialog box
Figure: Select Unit dialog box

Table: Select Unit Dialog Box

Component

Description

Quick filter

Type the name of the category or unit you are searching for. For more information, see Quick Filter .

Units

Select the category and unit of the value. For more information, see Units .

Prefix

Select the prefix of the unit.

Selected unit

Displays the defined unit with prefix.

  • Regional and Language Overview
  • Quick Filter
  • Units
  • Metric Prefixes
  • Precision Format
  • WorkStation does not Display Correct Values