earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : WebReports
Fonctionnalités : Rapports
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16/12/2021

Uploading a Report Pack

You upload a report pack to add new reports to the Report Server. The new reports display in the Reports folder in WorkStation, and in the Reports Tree of the WebReports Web site.

Afficher plus
action_close

Report packs contain reports. You can use report packs to upload new reports to WebReports, and to provide portability of reports from one Reports Server to another​.

New reports from Schneider Electric

Schneider Electric distributes new reports using report packs. When you receive the report pack, you use WebReports and upload the report pack to deploy the new reports to your Reports Server. Once deployed to your Reports Server, you can generate and view the reports in either WorkStation or the WebReports Web site.

Portable reports

Report packs provide a convenient and portable way of adding reports to your Reports Server. For example, suppose you have a collection of reports that reside on a Reports Server in location A and you want to add the collection to a Reports Server in location B. Using the WebReports Report Pack feature, you can select the reports that you want in the report pack. You then download the report pack to a media device such as a USB drive at location A. When you arrive at location B, you can upload the report pack to deploy the reports to the Reports Server where they become available in both WorkStation and the WebReports Web site.

Report Pack Size Restrictions

There is a limitation on the size of report pack you can upload or download to and from the Reports Server. If you attempt to upload or download a report pack of file size greater than 4 MB, an error message is displayed and you cannot complete the upload or download.

Report Packs and References

If you download a report pack and then upload the report pack to a Reports Server that has a new reports database, all object references are maintained except references to extended trend logs, EcoStruxure BMS server, and user parameters (these objects will not exist in the new system therefore the references will be incorrect). To avoid incorrect references, you can choose to exclude references to extended trend logs, EcoStruxure BMS server, and user parameters before you upload the report pack.

To upload a report pack
  1. In WebReports, on the menu bar, click Report Packs .

  2. In the Upload Report Pack box, enter the report pack that you want to upload.

    Déclaration

    You cannot upload a report pack with file size greater than 4 MB.

  3. To exclude references to extended trend logs, EcoStruxure BMS servers and users, select Exclude Object References . Pour plus d'informations, voir Report Packs .

  4. Click Upload .

  • Manage Report Packs Page
  • Report Packs