earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 3.2
15/10/2020

User Account Management Overview

arrow1_rotationUser Accounts and User Account Groups arrow1_rotationDomains arrow1_rotationSoftware Permissions arrow1_rotationLog on Methods arrow1_rotationWorkspace Management arrow1_rotationAutomatic Logoff arrow1_rotationGuest User Account arrow1_rotationAutomatic Logoff to Guest Account arrow1_rotationGuest Log On in WebStation

When logging on to an EcoStruxure BMS server, you have to authenticate yourself by using a valid user account. The user account has to belong to the same domain as the server you log on to.

The user account has to be a member of at least one user account group or be mapped through an active directory user account group. ​To restrict the user, software permissions are added to the user account group or to the individual user account. One or more customized workspaces can be connected to the user account group.

When logging on to the EcoStruxure BMS server that acts as the domain controller, in this example an Enterprise Server, you have access to all EcoStruxure BMS servers in the domain without using additional log on. If you log on to an individual EcoStruxure BMS server you have no access to other EcoStruxure BMS servers in the domain.

 
action_zoom_plus_stroke To log on to an EcoStruxure BMS server you have to use a valid user account that is located in the same domain as the EcoStruxure BMS server.
Figura: To log on to an EcoStruxure BMS server you have to use a valid user account that is located in the same domain as the EcoStruxure BMS server.

The EcoStruxure BMS considers a user account valid when:

  • The user account exists

  • The user account is not disabled or expired

  • The user account belongs to a user account group or mapped active directory user group

  • The user account group belongs to a domain

  • The user account has defined software permissions, either defined on the individual account or inherited from the user account group

User Accounts and User Account Groups

A user account can be a member of one or more user account groups and belongs to a particular domain.

Para obtener más información, consulte User Accounts and User Account Groups .

Domains

An EcoStruxure Building Operation domain contains user accounts, user account groups, software permissions, workspaces, and one or several EcoStruxure BMS servers. The EcoStruxure BMS server that hosts and administers the domain is called the domain controller.

Para obtener más información, consulte Domains .

Software Permissions

Software permissions are used to manage privileges that user account groups and user accounts own to objects in Building Operation software. In the EcoStruxure Building Operation software, you can assign two types of software permissions to user account groups and user accounts: path permissions and command permissions. You can also assign extended permissions to all the instances of folder structure or of a custom type.

Para obtener más información, consulte Software Permissions .

Log on Methods

The EcoStruxure BMS provides two methods to log on to the system. Either you log on as a Windows User with your Windows Active Directory user account or as EcoStruxure Building Operation user with your EcoStruxure Building Operation user account.

Para obtener más información, consulte Log On Methods .

Workspace Management

The workspace defines the content and layout of WorkStation. The content and layout of the workspace can be adapted different tasks for user accounts or user account groups.

Para obtener más información, consulte Workspace Management .

Automatic Logoff

The automatic logoff function makes it possible for the system to automatically log off a user after a specified time of inactivity.

Para obtener más información, consulte Automatic Logoff .

Guest User Account

You create a Guest user account when you need a limited view of the system that does not require any log on.

Para obtener más información, consulte Guest User Account .

Automatic Logoff to Guest Account

You can configure a user group to automatically log on to the Guest user account when a user account that belongs to the group is manually or automatically logged off.

Para obtener más información, consulte Automatic Logoff to Guest Account .

Guest Log On in WebStation

A guest logon is used when you want the user to get immediate access to the EcoStruxure Building Operation software using WebStation.

  • Function Overview
  • Software Permissions
  • Domains
  • User Accounts and User Account Groups
  • Log On Methods
  • Workspace Management
  • Automatic Logoff
  • Guest User Account
  • Automatic Logoff to Guest Account