earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/2/2024

User Action Properties

Use the User Action properties dialog box to configure the mandatory or required user actions items.

 
action_zoom_plus_stroke User action properties
Figure: User action properties

Table: User Action Properties

Component

Description

User action

Displays the user action item you are configuring.

Comment

Select True to require the users to write a comment when they perform this kind of user action.

Action note

Select True to require the users to add an action note to this kind of user action.

Cause note

Select True to require the users to report the circumstances of this kind of user action.

  • User Actions
  • Create Alarm Wizard – User Action Page