earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: WebReports
Funcionalidades: Relatórios
Versão do produto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16-12-2021

Users Groups Report

The Users Groups report provides information about the user accounts that are configured in the EcoStruxure Building Operation database. The report displays the user account name, the first and last name of the user, the E-mail address of the user, and the user groups of the user account. You can use the report when you need to identify the EcoStruxure Building Operation user accounts and their assigned user groups.

The following table shows the input parameters for the report.

Tabela: Users Groups Input Parameters

Input Parameters

Description

None

The Users Groups report does not prompt for filtering criteria. The report generates output regarding all user accounts that are configured in the EcoStruxure Building Operation database.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page