earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
Product version: 1.8, 1.9
12/17/2010

Using Full Screen Mode

You use full screen mode to maximize the Work area so that you get a better view.

Show More
action_close

​You can increase the Work area in WorkStation by using Full screen mode and hiding toolbars and panes.

Hide Toolbars and Panes

You can increase the work area in WorkStation by hiding some or all of the toolbars and panes. Most functions can still be reached using the right-click method. All toolbars and panes that are hidden can be displayed again at any time.

In this example, the System Tree pane, Address bar, Basic toolbar, and Main menu are hidden.

 
action_zoom_plus_stroke Default workspace (top left) and a workspace with the System Tree pane, Address bar, Basic toolbar, and Main menu hidden (bottom right).
Figure: Default workspace (top left) and a workspace with the System Tree pane, Address bar, Basic toolbar, and Main menu hidden (bottom right).

Full Screen Mode

To further increase the Work area you can use Full screen mode. This function maximizes the window in focus to fill the whole screen. This is a good function to use, for example, when you work in large graphics with lots of information.

 
action_zoom_plus_stroke Full screen mode
Figure: Full screen mode

To use full screen mode
  • In WorkStation, on the Main Menu , click View , and then click Full screen .

  • Increase the Work Area in WorkStation
  • Returning from Full Screen Mode