earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WorkStation
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Using Full Screen Mode

You use full screen mode to maximize the Work area so that you get a better view.

Visa mer
action_close

​You can increase the Work area in WorkStation by using Full screen mode and hiding toolbars and panes.

Hide Toolbars and Panes

You can increase the work area in WorkStation by hiding some or all of the toolbars and panes. Most functions can still be reached using the right-click method. All toolbars and panes that are hidden can be displayed again at any time.

In this example, the System Tree pane, Address bar, Basic toolbar, and Main menu are hidden.

 
action_zoom_plus_stroke Default workspace (top left) and a workspace with the System Tree pane, Address bar, Basic toolbar, and Main menu hidden (bottom right).
Figur: Default workspace (top left) and a workspace with the System Tree pane, Address bar, Basic toolbar, and Main menu hidden (bottom right).

Full Screen Mode

To further increase the Work area you can use Full screen mode. This function maximizes the window in focus to fill the whole screen. This is a good function to use, for example, when you work in large graphics with lots of information.

 
action_zoom_plus_stroke Full screen mode
Figur: Full screen mode

To use full screen mode
  • In WorkStation, on the Main Menu , click View , and then click Full screen .

  • Increase the Work Area in WorkStation
  • Returning from Full Screen Mode