earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2022, 2023, 2024
9/18/2024

Utilities

arrow1_rotationSignal Generator arrow1_rotationSimple Math Operators arrow1_rotationTimed Force Objects arrow1_rotationHTML Utilities arrow1_rotationJavaScript Utilities

The EcoStruxure Building Operation software is equipped with three types of utilities: Signal Generators, Simple Math Operators, and Timed Force objects. These utilities are used for testing, for example, trend logs and alarms.

For more information, see WorkStation .

Signal Generator

Signal Generator is used to create a sinusoidal, square, or saw tooth curve. Signal generator can also be used to generate a setpoint, an alarm, or an event.

Simple Math Operators

Simple Math Operator is used to add, subtract, multiply, and divide a one value from another.

Timed Force Objects

Timed Force objects are utility objects that force an override of the actual value of an analog, digital, or multistate output for a period of time specified either as a time duration or as a selected end date and time.

For more information, see Timed Force Objects .

HTML Utilities

The HTML utility object enables experienced software developers to embed custom web pages/applications inside the system.

For more information, see HTML Utilities .

JavaScript Utilities

The JavaScript utility object can be used by experienced software developers to increase reuse of JavaScript files.

For more information, see JavaScript Utilities .

  • WorkStation
  • Timed Force Objects
  • Creating a Utility Object
  • HTML Utilities
  • JavaScript Utilities