Building Operation handles values and numbers with the highest precision. By default, the unit of a value is converted according to the regional settings of the user’s operating system.
Building Operation supports both the SI metric system and the US Customary System for units of measurement.
There are four optional ways to display units:
As MS Windows
As configured in object
International System of Units (Metric)
United States Customary Units (US)
Per maggior informazioni, consulta Units .
WorkStation supports the metric prefix range from yocta (10 -24 ) to yotta (10 24 ). The use of a prefix is optional and is defined together with the unit.
Per maggior informazioni, consulta Metric Prefixes .
Values in Building Operation are stored in the Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.
Per maggior informazioni, consulta Precision Format .