Funzionalità: Localizzazione
Versione del prodotto: 3.2, 3.3, 2022
15/10/2020

Value Presentation

arrow1_rotationUnits arrow1_rotationMetric Prefixes arrow1_rotationPrecision Format

The EcoStruxure Building Operation software handles values and numbers with the highest ​precision. By default, the unit of a value is converted according to the regional settings of the user’s operating system.

Units

The EcoStruxure Building Operation software supports both the SI metric system and the US Customary System for units of measurement.

There are four optional ways to display units:

  • As MS Windows

  • As configured in object

  • International System of Units (Metric)

  • United States Customary Units (US)

Per maggior informazioni, consulta Units .

Metric Prefixes

​​WorkStation supports the metric prefix range from yocta (10 -24 ) to yotta (10 24 ). The use of a prefix is optional and is defined together with the unit.

Per maggior informazioni, consulta Metric Prefixes .

Precision Format

​Values in the EcoStruxure Building Operation software are stored in the EcoStruxure Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.

Per maggior informazioni, consulta Precision Format .

  • Regional and Language Overview
  • Units
  • Metric Prefixes
  • Precision Format