earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Variable Triggered Trend Log Properties – Basic Tab

Use the Basic tab to configure the Variable triggered trend log.

 
action_zoom_plus_stroke Variable triggered trend log properties - Basic tab
Figura: Variable triggered trend log properties - Basic tab

Tabla: Variable Triggered Trend Log Properties - Basic Tab

Component

Description

Status

Displays the status of the trend log.

Enabled

Displays True if the trend log is enabled.

Logged variable

Enter the variable you want to log.

Delta

Select the minimum value change that triggers a new record.

Trigger variable

Enter the variable that triggers the trend log to start recording.

Trigger condition

Select when you want the variable recorded: when the trigger variable changes to True, changes to False, or at all changes.

Para obtener más información, consulte Variable Triggered Trend Logs .

Log size

Select the number of records to store before old records are overwritten, including internal records generated by the trend log.

Para obtener más información, consulte Log Record Storage .

Clear when enabled

Select True to clear the trend log when it is enabled.

  • Variable Triggered Trend Logs
  • Trend Log Types
  • Configure Dialog Box – Configuration Tab
  • Configure Dialog Box – Operation Tab
  • Variable Triggered Trend Logs
  • Log Record Storage
  • General Information Properties – Basic Tab
  • References Tab
  • Missing Trend Log Records