功能: 趋势
产品版本: 1.8
2016/10/13

Variable Triggered Trend Logs

​The variable triggered trend log records the variable when the conditions of the associated trigger variable are met. Use this type of trend log when the log interval is scheduled to log monthly or yearly, or when another device is used to trigger the log.

For example, in the figure below, the variable triggered trend log records a variable every time the associated trigger variable, for example, a switch, changes to true. The records are printed in a trend chart. Notice that the variable triggered trend log records the variable without any regard to time or delta.

 
action_zoom_plus_stroke Variable triggered trend log schematic
图: Variable triggered trend log schematic

You can configure the trend log to collect data when the trigger value changes to True, changes to False, or All changes.

 
action_zoom_plus_stroke Trigger variable changes to true
图: Trigger variable changes to true
 
action_zoom_plus_stroke Trigger variable changes to false
图: Trigger variable changes to false
 
action_zoom_plus_stroke Trigger variable all changes
图: Trigger variable all changes
  • Trend Log Types
  • Trends Overview
  • Trend Units
  • Creating a Variable Triggered Trend Log
  • Configuring a Variable Triggered Trend Log
  • Variable Triggered Trend Log Properties
  • Log Record Storage