earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Device Administrator, Enterprise Central, Enterprise Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, Script Editor, Software Administrator
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Version Numbers and Parallel Installations

The EcoStruxure Building Operation software version number is constructed with four numbers, which represents different parts of the version: Major, Minor, Maintenance, and Build.

 
action_zoom_plus_stroke The EcoStruxure Building Operation version number structure
图: The EcoStruxure Building Operation version number structure

表格: The EcoStruxure Building Operation Version Number Structure

Version number

Description

Major

Increment when major functionality changes are released.

Minor

Increment when minor functionality changes are released.

Maintenance

Increment when correctional changes are released.

Build

A sequential number to guarantee uniqueness of the version release.

When installing a product with a higher version number than what is already installed, the installation package asks you if you want to upgrade or replace your current installation. When starting an installation package with the same version number as the software that is already installed, the installation package asks you whether you want to repair or reinstall the installation.

通知

数据丢失

Do not execute or run two different versions of a product simultaneously on your server or computer. Running parallel installations can cause data loss or corruption.

不遵照这些说明可导致数据丢失。

On the same computer or server, you can install products parallel to each other that have different major or minor version numbers. For example, you can install WorkStation 2.1.6.0 on a computer that already has version 1.2.1.0 installed. You have to use different installation folders for parallel versions.

重要:
  • You cannot install parallel License Administrators.

  • You should always run the latest maintenance version of the License Administrator or License Server for your EcoStruxure Building Operation version.

Version history log

The version history log contains the following information:

  • The EcoStruxure Building Operation versions that have been installed on the computer

  • The hotfix versions that have been installed on the computer

  • The date and time the installation was performed

  • The name of the Windows user account that performed the installation

The version log is created in the installation folder of each EcoStruxure Building Operation product. The name of the log file is: version_history.txt .

  • Installation Overview
  • Installation Reparation
  • Reinstallation
  • System Upgrade Overview