earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
5/18/2018

Viewing a Cause Note

You view a cause note to see what caused the alarm.

Show More
action_close

A cause note is a predefined note that contains information on what triggered the alarm. This information can be helpful the next time the same alarm is triggered.

In some cases, adding a cause note is optional. In other cases, you are required to add a cause note when you acknowledge the alarm. 

You add a cause note using WorkStation or WebStation. You can view a cause note added to an alarm in WorkStation or Webstation.

To view a cause note
  1. In Workstation, in the the System Tree pane, select the alarm.

  2. On the Actions menu, click View Cause Notes .

  • Cause Notes
  • Alarms Pane and Alarm View
  • Alarm Comments
  • Alarms Pane Context Menu
  • Adding a Comment to an Alarm
  • Alarms Pane and Alarm View Toolbar