earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WorkStation
功能: 警报
产品版本: 2024, 7.0
2024/12/2

Viewing a Cause Note

You view a cause note to see what caused the alarm.

显示更多
action_close

A cause note is a predefined note that contains information on what triggered the alarm. This information can be helpful the next time the same alarm is triggered.

In some cases, adding a cause note is optional. In other cases, you are required to add a cause note when you acknowledge the alarm. 

You add a cause note using WorkStation or WebStation. You can view a cause note added to an alarm in WorkStation or Webstation.

To view a cause note
  1. In Workstation, in the the System Tree pane, select the alarm.

  2. On the Actions menu, click View Cause Notes .

  • Cause Notes
  • Alarms Pane and Alarm View
  • Alarm Comments
  • Alarms Pane Context Menu
  • Adding a Comment to an Alarm
  • Alarms Pane and Alarm View Toolbar