earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 1.8, 1.9
5/24/2011

Viewing a Schedule

You view a schedule to add, remove, or edit events.

Show More
action_close

The Schedule Editor serves as a workspace to plan and design a schedule. You use this editor to create, manage, and display weekly scheduled events and exception events.

All edits done in the editor will take effect as soon as they are added. To help you avoid mistakes, WebStation warns you when you make changes in a schedule for today’s date.

Note:

You can only view Xenta Central schedules in the Schedule Editor in WebStation.

The following figure displays the schedule of the lights within the building. The weekly events are in light grey and the exception event in light green. The values of the events are also displayed. Monday, September 19 is an exception event, so it does not follow the same scheduled events as the rest of the week. The lights are off all day. For the rest of the week, the lights turn on at 07:00 and turn off at 18:00.

 
action_zoom_plus_stroke Schedule Editor
Figure: Schedule Editor

To view a schedule
  • In WebStation, in the System Tree pane, select the schedule you want to view.

The schedule is displayed in the Schedule workspace.

  • Schedule Editor in WebStation
  • How Schedules Work
  • Schedule Workspace