Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.8
13/10/2016

Viewing Shortcuts

You view shortcuts to objects in the System Tree pane when you want to see non-presentation objects, for example Script or Function Block programs. By default, non-presentation objects are hidden in the System Tree pane.

Mostrar más
action_close

Shortcuts without targets and shortcuts to objects are non-presentation objects. By default, non-presentation objects are not displayed in the System Tree, except when selected by means of the System Tree filter. However, a shortcut with a SmartStruxure server or a folder as a target is a presentation object and is always displayed in the System Tree.

When a shortcut is created in a SmartStruxure server or folder by means of the File-New submenu or the New-Shortcut command of the Context menu, the shortcut has no valid target. In this case, only the overlay icon (a small arrow in a square) is displayed (because no target type is assigned).

 
action_zoom_plus_stroke Example of a shortcut without an assigned target
Figura: Example of a shortcut without an assigned target

When a target is assigned, the overlay icon of the shortcut is added on top of the icon of the target. Para obtener más información, consulte Shortcut Properties – Basic Tab .

The following figure is an example of a shortcut for an analog value in the System Tree:

 
action_zoom_plus_stroke Example of a shortcut to an analog value
Figura: Example of a shortcut to an analog value

When you click a shortcut, the address of the shortcut is displayed in the address bar and the name of the shortcut is displayed in the the tab of the shortcut window.

To view shortcuts to objects
  • In the System Tree pane, click the Show/Hide non-presentation objects button

     
    action_zoom_plus_stroke
    .

You can now view the properties of the shortcut(s).

  • Viewing Shortcut Properties
  • Shortcut Presentation