earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/9/4

Viewing Shortcuts

You view shortcuts to objects in the System Tree pane when you want to see non-presentation objects, for example Script or Function Block programs. By default, non-presentation objects are hidden in the System Tree pane.

显示更多
action_close

Shortcuts without targets and shortcuts to objects are non-presentation objects. By default, non-presentation objects are not displayed in the System Tree, except when selected by means of the System Tree filter. However, a shortcut with an EcoStruxure BMS server or a folder as a target is a presentation object and is always displayed in the System Tree.

When a shortcut is created in an EcoStruxure BMS server or folder by means of the File-New submenu or the New-Shortcut command of the Context menu, the shortcut has no valid target. In this case, only the overlay icon (a small arrow in a square) is displayed (because no target type is assigned).

 
action_zoom_plus_stroke Example of a shortcut without an assigned target
图: Example of a shortcut without an assigned target

When a target is assigned, the overlay icon of the shortcut is added on top of the icon of the target. 有关更多信息,请参阅 Shortcut Properties – Basic Tab .

The following figure is an example of a shortcut for an analog value in the System Tree:

 
action_zoom_plus_stroke Example of a shortcut to an analog value
图: Example of a shortcut to an analog value

When you click a shortcut, the address of the shortcut is displayed in the address bar and the name of the shortcut is displayed in the the tab of the shortcut window.

To view shortcuts to objects
  • In the System Tree pane, click the Show/Hide non-presentation objects button

     
    action_zoom_plus_stroke
    .

You can now view the properties of the shortcut(s).

  • Viewing Shortcut Properties
  • Shortcut Presentation