WebReports Schedules provide a way for you to automatically generate a dashboard report at specified times and days. You create a report schedule using the Schedules menu option at the WebReports Web site.
Using the Schedules settings, you can perform the following tasks:
Create a schedule
Edit a schedule
Specify the frequency for running the scheduled report
Specify start dates and times for running the schedule
Select a format for the scheduled report output
Select a destination for the scheduled report output
Disable a schedule temporarily
You can only schedule dashboard reports with Schedules. For more information, see Dashboard Reports .
You can specify how often you want a schedule to run, for example weekly or monthly, or perhaps just once.
For more information, see Report Schedule Frequency .
You can copy the settings of one schedule and use them to provide the settings for another schedule, when you want to run a different scheduled report.
For more information, see Report Schedule Modifications .