earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: WebReports
Funzionalità: Report
Versione del prodotto: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16/12/2021

Schedules for Dashboard Reports

WebReports Schedules provide a way for you to automatically generate a dashboard report at specified times and days. You create a report schedule using the Schedules menu option at the WebReports Web site.

Using the Schedules settings, you can perform the following tasks:

  • Create a schedule

  • Edit a schedule

  • Specify the frequency for running the scheduled report

  • Specify start dates and times for running the schedule

  • Select a format for the scheduled report output

  • Select a destination for the scheduled report output

  • Disable a schedule temporarily

You can only schedule dashboard reports with Schedules. Per maggior informazioni, consulta Report dashboard .

Report Schedule Frequency

You can specify how often you want a schedule to run, for example weekly or monthly, or perhaps just once.

Per maggior informazioni, consulta Report Schedule Frequency .

Report Schedule Modifications

You can copy the settings of one schedule and use them to provide the settings for another schedule, when you want to run a different scheduled report.

Per maggior informazioni, consulta Report Schedule Modifications .

  • Report dashboard
  • Report Schedule Frequency
  • Report Schedule Modifications