Use the Building Operation WorkStation window to log on to WorkStation.
Component |
Description |
U ser name |
Type the user name of your EcoStruxure Building Operation user account. For more information, see User Accounts and User Account Groups . |
Password |
Type the password of your EcoStruxure Building Operation user account or of your Windows user account. |
Domain |
Type the name of the EcoStruxure Building Operation domain that you want to log on to. If you do not enter a domain, you are logged on to the local domain. For more information, see Domains . |
Server |
Select the Server hypertext transfer protocol option for communication with the EcoStruxure BMS server. Enter an EcoStruxure BMS server name or an IP address for the EcoStruxure BMS server you want to log on to. |
Log on as |
Click to log on to WorkStation with your Windows user account. For more information, see User Accounts and User Account Groups . |
Remember me on this computer |
Select to save the entered information. The information is automatically filled in the next time you log on. |
Log on |
Click to log on to WorkStation. |
Click here to learn more about Building Operation |
Click to open the WebHelp home page. For more information, see WebHelp Overview . |