The WebReports installation requires you to select certain roles and services to install on the Application Server and the Web Server (IIS), and to install .NET Framework 3.5 and .NET Framework 4.5 features. You install these roles and features using the Server Manager in Windows Server 2008, Windows Server 2012, or Windows Server 2012 R2. For Windows 7, Windows 8.1, and Windows 10, you configure IIS using Control Panel. It is recommended that you install these roles and features before you install SQL Server.
Server Manager is accessible from the Start screen or from the desktop (task bar). You begin by adding the .NET Framework 3.5 features, the IIS server role and selecting the role services, and then you add .NET Framework 4.5 features. The following figures show the features that must be selected when configuring Roles and Features for Windows Server 2012 or Windows Server 2012 R2 and IIS configuration for Windows 7, Windows 8.1, or Windows 10.
To Install .NET Framework 3.5 on Windows 8.1 or Windows 10 and Windows Server 2012 or Windows Server 2012 R2, enter the following source path:
dism /online /enable-feature /featurename:NetFX3 /all /Source:e:\sources\sxs /LimitAccess
In this example, the Windows Server 2012 setup CD is in the e drive. Use the appropriate drive in the path for your PC configuration.
For Windows Server 2008, you begin by adding the IIS server role and selecting the role services, and then you add the .NET Framework 3.5.1 features. The following figures show the settings that must be selected when configuring windows roles and features.
For Windows 7, Windows 8.1, and Windows 10, you can configure IIS using Control Panel. In Control Panel, navigate to Programs , and select Turn Windows features on or off . Select Internet Information Services to configure IIS.