Use the Workspace properties to configure the properties of a workspace.
Component |
Description |
![]() |
Add Click to add a pane to the workspace. For more information, see Create Object Wizard – Naming the Object Page . |
![]() |
Edit Click to edit a workspace pane. For more information, see Pane Properties . |
![]() |
Remove Click to remove a workspace pane. |
Menu |
Select Visible to show the menu in the workspace. |
Toolbar |
Select Visible to show the toolbar in the workspace. |
Address bar |
Select Visible to show the address bar in the workspace. |
Status bar |
Select Visible to show the status bar in the workspace. |
Search bar |
Select Visible to show the search bar in the workspace. |
History bar |
Select Visible to show the history bar in the workspace. |
Root path |
Enter the path for the workspace component. |