earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 2024, 7.0
12/2/2024

Workspace Properties

Use the Workspace properties to configure the properties of a workspace.

 
action_zoom_plus_stroke Workspace properties
Figure: Workspace properties

Table: Workspace Properties

Component

Description

 
action_zoom_plus_stroke

Add

Click to add a pane to the workspace. For more information, see Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit a workspace pane. For more information, see Pane Properties .

 
action_zoom_plus_stroke

Remove

Click to remove a workspace pane.

Menu

Select Visible to show the menu in the workspace.

Toolbar

Select Visible to show the toolbar in the workspace.

Address bar

Select Visible to show the address bar in the workspace.

Status bar

Select Visible to show the status bar in the workspace.

Search bar

Select Visible to show the search bar in the workspace.

History bar

Select Visible to show the history bar in the workspace.

Root path

Enter the path for the workspace component.

  • Workspace Components and Customization
  • Pane Properties
  • Workspace Layout Changes Have Disappeared
  • General Information Properties – Basic Tab
  • Pane Properties
  • Create Object Dialog – Naming the Object Page