Use the Pane configuration page to determine the layout of the component you are adding to the workspace.
Component |
Description |
Show toolbar |
Select No to hide the component toolbar. |
Default dock position |
Select a default dock position in the workspace for the component. |
Default visibility |
Select Hidden to hide the component. |
Display name |
Type the pane name that is to be displayed. Display name is available only in WorkStation. |
Initial path |
Click to change the location of the component. Mer information finns i Workspace Wizard – Workspace Configuration Page . |