earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2.0, 2.1, 3.0, 3.1
2018/12/14

Workspace Wizard – Pane Configuration Page

Use the Pane configuration page to determine the layout of the component you are adding to the workspace.

 
action_zoom_plus_stroke Pane configuration page
图: Pane configuration page

表格: Pane Configuration Page

Component

Description

Show toolbar

Select No to hide the component toolbar.

Default dock position

Select a default dock position in the workspace for the component.

Default visibility

Select Hidden to hide the component.

Display name

Type the pane name that is to be displayed. Display name is available only in WorkStation.

Initial path

Click to change the location of the component. 有关更多信息,请参阅 Workspace Wizard – Workspace Configuration Page .

  • Workspace Components and Customization
  • Create Object Wizard – Naming the Object Page
  • Workspace Wizard – Workspace Configuration Page