earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 1.8
13/10/2016

Workspace Wizard – Workspace Configuration Page

Use the Workspace configuration page to add, edit, and remove workspace components.

 
action_zoom_plus_stroke Workspace configuration page
Figura: Workspace configuration page

Tabla: Workspace Configuration Page

Component

Description

Menu

Select Visible to show the menu in the workspace.

Address bar

Select Visible to show the address bar in the workspace.

Search bar

Select Visible to show the search bar in the workspace.

Toolbar

Select Visible to show the toolbar in the workspace.

Status bar

Select Visible to show the status bar in the workspace.

History bar

Select Visible to show the history bar in the workspace.

Root path (Applies to Address Bar and System Tree)

Enter the path to the workspace component.

Listed components

Lists the standard components included in the workspace. Select a component and click the Add , Edit or Remove button.

 
action_zoom_plus_stroke

Click to add a new component to the workspace. Para obtener más información, consulte Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke

Click to edit a component. The workspace properties pane is displayed. Para obtener más información, consulte Pane Properties .

 
action_zoom_plus_stroke

Click to remove a component.

  • Workspace Components and Customization
  • Create Object Wizard – Naming the Object Page
  • Workspace Properties
  • Pane Properties
  • Create Object Wizard – Naming the Object Page