earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: ​License Administrator, ​License Server
Functionalities: License Management
Product version: 1.9, 2.0, 2.1, 3.0, 3.1
12/14/2016

​WorkStation and Client Tools Address Configuration

After licenses are activated on the License Server you have to configure the Workstation and its client tools connection to the License Server, where licenses are available for check out. The address to the License Server is defined either during the installation of WorkStation, through License Administrator, or Windows registry.

 
action_zoom_plus_stroke WorkStation configuration and check in/out of client station network license and client tool network licenses
Figure: WorkStation configuration and check in/out of client station network license and client tool network licenses

Table: WorkStation Configuration

Number

Description

1

Configure the WorkStation and client tool address to the License Server.

2

Remove any activated local licenses.

3

When you logon to WorkStation or start a client tool, the required license is automatically checked out from the License Server.

A checked out network license is not physically moved to or activated on WorkStation. The client station and client tool licenses remain in the License Server but are allocated to the dedicated WorkStation. The license is therefore not available for other WorkStations to check out.

  • Network License Management
  • Enterprise Server Address Configuration
  • License Management
  • License Administrator
  • License Server Address View
  • Configuring the Address to the License Server