earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestão de utilizadores
Versão do produto: 3.2, 3.3, 2022
15-10-2020

User Account – Summary Tab

Use the Summary tab to edit the basic settings for a user account. For example, you can enable or disable the user account, or change the password for the account.

 
action_zoom_plus_stroke Summary tab
Imagem: Summary tab

Tabela: Summary Tab

Component

Description

Expires on

Enter an expiration date and time for the user account. By default, there is no expiration date for the account.

Disabled

Select True to disable the user account.

Force password change

Select True to force the user to change password after the initial logon.

Password

Type the password again.

Confirm password

Type the password again.

  • User Accounts and User Account Groups
  • User Account Wizard – General Page
  • Password Policy