earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 2024, 7.0
03/12/2024

Domain Properties

Use the Domain properties to configure the properties of a domain.

 
action_zoom_plus_stroke Domain properties
Figura: Domain properties

Tabla: Domain Properties

Component

Description

Maximum logon attempts

Select the maximum number of failed logon attempts that a user can make before WorkStation is temporarily locked.

Password

Type the password EcoStruxure BMS servers ​internally use to enhance the EcoStruxure BMS server communication security in the domain.

Confirm Password

Type the password EcoStruxure BMS servers ​internally use to enhance the EcoStruxure BMS server communication security in the domain.

Windows domain name

Type the name of the Windows domain where the Windows Active directory is located from which you want to map user account groups. Para obtener más información, consulte Windows Active Directory User Groups .

  • Domains
  • General Information Properties – Basic Tab
  • EcoStruxure BMS Server Communication