earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2024, 7.0
2024/12/3

Domain Properties

Use the Domain properties to configure the properties of a domain.

 
action_zoom_plus_stroke Domain properties
图: Domain properties

表格: Domain Properties

Component

Description

Maximum logon attempts

Select the maximum number of failed logon attempts that a user can make before WorkStation is temporarily locked.

Password

Type the password EcoStruxure BMS servers ​internally use to enhance the EcoStruxure BMS server communication security in the domain.

Confirm Password

Type the password EcoStruxure BMS servers ​internally use to enhance the EcoStruxure BMS server communication security in the domain.

Windows domain name

Type the name of the Windows domain where the Windows Active directory is located from which you want to map user account groups. 有关更多信息,请参阅 Windows Active Directory User Groups .

  • Domains
  • General Information Properties – Basic Tab
  • EcoStruxure BMS Server Communication