earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 3.2, 3.3, 2022
10/15/2020

Domain – Summary Tab

Use the Summary tab to edit the description and domain controller password for a domain.

 
action_zoom_plus_stroke Summary tab
Figure: Summary tab

Table: Summary Tab

Component

Description

Description

​Type a description of the object.

Windows domain name

Type the name of the Windows domain where the Windows Active directory is located from which you want to map user account groups. For more information, see Windows Active Directory User Groups .

Domain Controller

​Displays the path and name of the domain controller.

  • Domains
  • Domain Wizard – Authentication Page
  • Windows Active Directory User Groups