earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
5
Ratgeber

Ratgeber


Produkte: License Administrator, License Server
Funktionen: Lizenzverwaltung
Produktversion: 1.8, 1.9
23.05.2015

Repairing a Network License

You repair damaged network licenses so they become available to check out by WorkStations, client tools, and Enterprise Servers.

Mehr zeigen
action_close

A license can in several ways become damaged. Use the License Administrator to repair a damaged network license on the License Server where the damaged license is located. Local licenses cannot be repaired. Instead you have to remove the damaged local licenses and reactivate the licenses from new license files.

Licenses can be damaged by the following actions:

  • Copying licenses from one system to another. This is an illegal action.

  • Restoring a License Server backup.

  • Adjusting the system clock to an earlier time.

  • Restoring the system to correct system problems or roll back changes.

  • Changing the Enterprise Server, License Server or WorkStation hardware component.

Hinweis
  • Repairing a network license requires access to the Internet.

  • You are only allowed to repair a license four times a year.

  • All repair actions are registered by the Activation Server and are traceable.

 
action_zoom_plus_stroke Damaged network license
Abbildung: Damaged network license

To repair a network license
  1. In License Administrator, click the Licenses view.

  2. Select the network license that you want to repair.

     
    action_zoom_plus_stroke
  3. On the Licenses toolbar, click the Repair license button

     
    action_zoom_plus_stroke
    .

  4. Click Yes .

     
    action_zoom_plus_stroke
  5. Click Close .

     
    action_zoom_plus_stroke
  6. Click Restart now , to restart the License Server and make the repaired licenses ​available for checkout.

     
    action_zoom_plus_stroke

The license is now repaired and available to be checked out.

  • License Repair
  • Licenses View Icons
  • Licenses View