earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : WebStation
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
22/07/2018
Cliquez pour afficher la version mise à jour qui n'a pas encore été traduite

Modification du mot de passe

Vous devez modifier régulièrement votre mot de passe utilisateur EcoStruxure Building Operation afin d'en garantir la confidentialité.

Afficher plus
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure Building Operation functions.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure Building Operation account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure Building Operation account and the Windows account is provided by the system administrator.

Déclaration

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Pour plus d'informations, voir EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both Building Operation users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

Pour modifier votre mot de passe
  1. Dans WebStation, dans le menu Réglages , sélectionnez Options , puis Changer le mot de passe .

  2. Dans la boîte de dialogue Changer le mot de passe , dans le champ Ancien mot de passe , saisissez votre ancien mot de passe

  3. Dans le champ Nouveau mot de passe , saisissez le nouveau mot de passe.

  4. Dans le champ Confirmer le mot de passe , saisissez à nouveau votre mot de passe.

  5. Cliquez sur OK .

  • Log on to WorkStation or WebStation
  • Change Password Dialog Box
  • Connexion à WebStation
  • Déconnexion de WebStation