You log on to WorkStation as another user than the current Windows user logged on to the computer to securely access the functions in the EcoStruxure BMS.
Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Mer information finns i EcoStruxure Building Operation Software Licensing Installation and Location .
In WorkStation, in the User name box, type the name of the Windows user account you want to use to log on.
In the Password box, type the Windows password for the user account.
In the Domain box, type a Windows domain name. If you do not enter a domain name, you are logged on to the local domain as an EcoStruxure Building Operation User.
Select the HTTPS protocol option for communication with the EcoStruxure BMS server.
In the Server box, enter an EcoStruxure BMS server name or an IP address.
You can also, in the scroll down menu, choose a server host name from the list. When you start typing the host name or the IP number of the server, you will be offered suggestions from the saved list.
When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.
Select Remember me on this computer to have WorkStation remember your settings.
Click Log on .
In the Registering Your System Online dialog box, you can register the system now or later:
Click Register now to register your system. Mer information finns i System Registration .
Click Register later to skip registration and register at a later time.