Use the Trend Chart Series menu to hide a series in the trend chart, to remove a series from the trend chart, change the settings for a series, and to view the properties for a series.
Command |
Description |
Visible |
Click (select or clear the check box) to show or hide the series in the trend chart. |
Settings |
Click to open the Trend Chart Settings dialog box, where you can change the settings for the series. Więcej informacji zawiera Trend Chart Settings Dialog Box – Left Axis Tab . Więcej informacji zawiera Trend Chart Settings Dialog Box – X Axis Tab . |
Remove |
Click to remove the series from the trend chart. |
Properties |
Click to open the Properties dialog box, where you can view the properties for the series. |