earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Trendy
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2021-07-20

Configuring the X-axis with a Relative Time Span

You configure the trend chart time span of the X-axis relative to the series current end point time to automatically adapt the trend chart to display the current time and the latest records within the specific time span.

Pokaż więcej
action_close

The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year​.

 
action_zoom_plus_stroke Absolute time span and relative time span, schematic
Rysunek: Absolute time span and relative time span, schematic

The y-axis refers to the measurement unit that the variable represents. The scale of the y-axis can be set manually or by auto scale. You can configure the trend chart to present series on one y-axis or two y-axes, one to the left and one to the right. Use two y-axes to present series with different ranges in the same trend chart.

 
action_zoom_plus_stroke One y-axis and two y-axes, schematic
Rysunek: One y-axis and two y-axes, schematic

To make reading easier, grid lines can be shown in the trend chart. Grid lines can be shown in both the x- and y-direction, independent of each other.

 
action_zoom_plus_stroke Grid lines, schematic
Rysunek: Grid lines, schematic

To configure the X-axis with a relative time span
  1. In WebStation, in the System Tree pane, select the trend chart you want to configure.

  2. On the Trend Chart toolbar, click the Settings button

     
    action_zoom_plus_stroke
    .

  3. In the Settings dialog box, click the X axis tab.

  4. In the Time mode box, select Relative (to current time) .

  5. In the Time span box, enter the time span.

  6. Click OK .

  7. Click Save .

The X-axis is now configured with a time span relative to current time.

  • Trend Chart Axes in WebStation
  • Configuring the X-axis with an Absolute Time Span
  • Showing Trend Chart Grid Lines
  • Manually Configuring the Y-Axis Scale
  • Automatically Configuring the Y-axis Scale
  • Saving Current Trend Chart Settings
  • Trend Chart View
  • Trend Chart Toolbar
  • Trend Chart Settings Dialog Box – X Axis Tab