earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Basic Functionality
Product version: 1.8, 1.9
3/17/2016

Forcing a Value

You force a value when you want to override a value, such as a value from a device.

Show More
action_close

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. For more information, see Timed Force Objects . When you release a forced value, the value returns to its normal status.

A forced value is indicated by orange color in the properties dialog boxes. In the List View and in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

You can view the unforced value, which is the real value from the system, at any time. For more information, see Viewing an Unforced Value .

To force a value
  1. In WebStation, click the value you want to force.

  2. In the value row, click Force .

  3. Click the Apply button

     
    action_zoom_plus_stroke
    .

The forced value is indicated by orange color.

  • Forced Values
  • Releasing a Forced Value