earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2022
2021-12-17

Releasing a Forced Value

You release a forced value to return it to its normal status.

Pokaż więcej
action_close

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. Więcej informacji zawiera Timed Force Objects .

When you release a forced value, the value returns to its normal status.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Więcej informacji zawiera Viewing an Unforced Value .

Indication in WorkStation

A forced value is indicated by orange color in the properties dialog boxes. In in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

In the List View and Search View, a forced value is indicated by the text [Forced] in the 'Value' column.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Więcej informacji zawiera Viewing an Unforced Value .

Indication in WebStation

A forced value is indicated by orange color and a pointing hand in the List view.

Indication in Function Block Graphics Viewer

A forced value is indicated by orange color in Function Block Graphics Viewer. Więcej informacji zawiera Forced Value Indication in Function Block Graphics Viewer .

To release a forced value
  1. In WebStation, click the value you want to release.

  2. In the value row, click Unforce .

  3. Click Save .

  • Forced Values
  • Forcing a Value