earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 基本功能
产品版本: 1.8, 1.9
2017/8/19

释放强制值

您可以释放强制值以返回其正常状态。

显示更多
action_close

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

A forced value can be released at any time. When you release a forced value, the value returns to its normal status.

A forced value is indicated by orange color in the properties dialog boxes. In the List View and in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

You can view the unforced value, which is the real value from the system, at any time. 有关更多信息,请参阅 浏览非强制值 .

释放强制值
  1. 在 WebStation 中,点击您想要释放的值。

  2. 在值行中,点击 强制

  3. 点击 应用 按钮

     
    action_zoom_plus_stroke

非强制值以它的原始颜色显示。

  • Forced Values
  • 强制值