earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Basic Functionality
Product version: 2022, 2023, 2024, 7.0
12/10/2024

Building Operation WebStation Window

Use the Building Operation WebStation window to log on to WebStation.

 
action_zoom_plus_stroke Building Operation WebStation Window
Figure: Building Operation WebStation Window

Table: Building Operation WebStation Window

Component

Description

User name

Type the user name.

Password

Type the password.

Domain

Type the name of the domain you want to log on to. If you do not enter a domain, you log on to the EcoStruxure BMS server local domain. For more information, see Domains .

Log on

Click to log on to WebStation.

Log on as guest

Click to log on as guest. This button is only available if a guest account is configured. For more information, see Guest User Account .

Log on with SSO

Click to log on with SSO. This button is only available if a SSO is available using Federated Authentication. For more information, see Federated Authentication .

Click here to learn more about Building Operation

Click to open the WebHelp home page. For more information, see WebHelp Overview .

  • Log on to WorkStation or WebStation
  • Guest User Account
  • Federated Authentication