earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Schedules
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
5/18/2018

Schedule Event Properties Dialog Box – Weekly View

Use the Weekly View in the Schedule Event Properties dialog box to create a new weekly event for an existing schedule.

 
action_zoom_plus_stroke Schedule event properties dialog box – Weekly view
Figure: Schedule event properties dialog box – Weekly view

Table: Schedule Event Properties Dialog Box – Weekly View

Component

Description

All Day

Select to create an all day event.

Value

Enter a value for the exception event.

At

Enter the start time for the exception event.

Until

Enter the end time for the exception event.

  • Weekly Events in WebStation
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calculated Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View