earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Schedules
Product version: 1.8, 1.9
2/3/2014

Schedule Event Properties Dialog Box – Calculated Exception View

Use the Calculated Exception View in the Schedule Event Properties dialog box to schedule recurring exceptions.

 
action_zoom_plus_stroke Schedule event properties dialog box – Calculated exception view
Figure: Schedule event properties dialog box – Calculated exception view

Table: Schedule Event Properties Dialog Box – Calculated Exception View

Component

Description

Event type

Click Exception to display the exception types.

Exception type

Select Calculated for an exception type to apply the schedule.

All Day

Select All Day for an all day event.

Start time

Double-click and type a start time for the exception event.

End time

Double-click and type an end time for the exception event.

Value

Double-click and type a value for the exception event.

Name

Type a name for the event.

Priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Year

Displays the current year, which is the default for the Calculated exception view.

Month

Select a month for the exception event or Odd month , Even month , Any month .

Week of month

Select a week of the month for the exception event or First , Second , Third , Fourth , Fifth , Last , Any week .

Day of week

Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  • Exception Events in WebStation
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View