earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018/9/28

Deleting a Backup Set from an Enterprise Server or Enterprise Central

You delete a backup set from the db_backup folder of the Enterprise Server or Enterprise Central when you no longer need the backup set.

显示更多
action_close

Backup sets are compressed backup files used for restoring data. The EcoStruxure Building Operation software stores the local backup set for an Enterprise Server or SmartX servers in the Local folder within the Backup sets folder.

Backup Sets Location

Backup sets are stored in different locations for stand-alone systems and multi-server systems.

有关更多信息,请参阅 Location of Backup Sets .

Backup Sets and Server Name

The EcoStruxure Building Operation software associates each backup set with a particular EcoStruxure BMS server name. Therefore, you should not rename an EcoStruxure BMS server unless absolutely necessary. If you do rename an EcoStruxure BMS server, the previous backup sets do not display in the Restore Options dialog box. You can view all the backup sets that are stored locally on an Enterprise Server. 有关更多信息,请参阅 Locating the Local Backup Path on the Enterprise Server or Enterprise Central .

提示:

Going forward, you must create new backups for the renamed EcoStruxure BMS server.

Backup Set Storage and Protection

EcoStruxure BMS servers store backup sets in their local directories. By design, the average user may not easily locate these backup directories using a Windows-based file system. For convenience, you can save backup sets stored on EcoStruxure BMS servers to WorkStation. After saving the backup set, you can also copy the file to another backup storage location.

有关更多信息,请参阅 Backup Set Storage and Protection .

Backup Set Import from WorkStation

You import a backup set from WorkStation to replace a lost or incomplete backup set, or to add a backup set to a new EcoStruxure BMS server.

有关更多信息,请参阅 Backup Set Import from WorkStation .

Automatic Purge of Backup Sets

An Enterprise Server stores multiple local and remote backup sets. As a result, these sets can consume much needed space on the Enterprise Server. To resolve this problem, you can configure the Enterprise Server to remove outdated backup sets.

有关更多信息,请参阅 Automatic Purge of Backup Sets .

To delete a backup set from the Enterprise Server or Enterprise Central
  1. In WorkStation, in the System Tree pane, select the Enterprise Server or Enterprise Central you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup and Restore Manager .

  4. In the Backup and Restore Manager , in the Backup sets path box, copy the entire backup sets path of the Enterprise Server.

  5. Open a browser, such as Windows Explorer.

  6. In the browser Address box, paste the backup sets path and press Enter .

  7. In the db_backup folder, open the ASArchives or LocalBackup folder.

  8. Right-click on the backup set that you want to delete and click Delete .

  9. Click Yes to remove the backup set.

  • Backup Sets
  • Control Panel Tab
  • Backup and Restore Manager on the Enterprise Server
  • Backup Set Storage and Protection