Use the Alarm View Settings submenu to change the way alarms are presented.
Command |
Description |
Display Alarm View on alarm |
Click to display an Alarm View in a new window when an alarm is triggered. Mer information finns i Displaying an Alarm View when an Alarm is Triggered . |
Edit standard filter |
Click to open the Select Conditions dialog box, where you sort out the information in the Alarms pane or an Alarm View. Mer information finns i Select Conditions Dialog Box . |
Save as standard layout |
Click to save the current Alarms pane or Alarm View layout as the standard layout for all users and for the Alarms pane or the specific Alarm View. |
Reset standard layout to factory default |
Click to reset the Alarms pane or Alarm View standard layout to factory default. |
Add/Remove columns |
Click to open the Add/Remove columns dialog box to add or remove columns from the Alarms pane or Alarm View. Mer information finns i Add/Remove Columns Dialog Box . |
Properties |
Click to open the Alarm View properties dialog box to view and edit the properties of the Alarms pane or Alarm View. Mer information finns i Alarm View Properties . |
Alarm state sort order |
Click to open the Alarm state sort order dialog box to determine how alarms will be sorted when the column State is used for sorting the alarms in the Alarms pane or an Alarm View. Mer information finns i Changing the Alarm State Sort Order . |
Detail view |
Click to open a detailed view for the selected alarm. Mer information finns i Alarm and Event Detail View . |